This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

WEBENCH® Tools/TPS560430: Understanding efficiency of WEBENCH Design with TPS560430

Prodigy 10 points

Replies: 1

Views: 52

Part Number: TPS560430

Tool/software: WEBENCH® Design Tools

Hello,

I created a WEBENCH Design using the TPS560430. With the following specs:

- Vin: 16.2V to 19.8V

- Vout: 3.3V

- Iout: 0.5A

I'm getting an efficiency of 81.3% however according to the data sheet (Page 7, Figure 1) I should be getting closer to 85% efficiency. Could you help explain to me why this is the case?

Thank you for the help!

  • Hi Noah,

    Thanks for reaching us out. Webench uses complex algorithms to estimate the efficiency and other operating values. We try our best to match with bench data with same bill of material (BOM).

    In this case, there might be a difference in BOM used in datasheet and Webench. This usually happens when Webench tries to give best possible solutions (considering cost/efficiency/footprint ). If we select different Inductor from alternate parts with lower DCR on Webench, you will find small jump in efficiency. 

    Best Regards,

    Bhushan       

       

    If my reply answers your question please click the "This resolved my issue" button

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.