This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00120: LED Status Indications for Battery, Panel and Load

Part Number: TIDA-00120
Other Parts Discussed in Thread: MSP430F5132

Hi,

I am using TIDA-00120 refrence design for 12V/10A MPPT Charge controller. I would like to use  P2.4, P2.5 and P2.6 pins of MSP430 for the LED Indications. In this i am not using GUI/ launch pad to connect to the PC. 

I tried to write the Firmware to config the Pins P2.4, P2.5 and P2.6. But i am unable to make the pins either "High". or "Low".

So please suggest me how to config above mentioned pins to use as GPIO pins.

Regards

Naresh