• TI Thinks Resolved

TIDA-00554: TIDA-00554

Prodigy 10 points

Replies: 1

Views: 14

Part Number: TIDA-00554

Can I get support to build a spectrometer using TI products from the scratch?

  • Prahlda,

    Welcome to the E2E forums, and thanks for your interest in our DLP technology.

    If you want to design a spectrometer using DLP, we recommend you refer to the reference design linked here:

    https://www.ti.com/tool/TIDA-00554

    This will provide you with schematics and drawings which will help with implementation of our electronics into a custom board. You can also purchase the EVM as a means to evaluate the chipset itself.

    I hope this helps.

    Regards,

    Philippe Dollo

    If a post answers your question, please click the "Verify Answer" button.