Other Parts Discussed in Thread: MSP-EXP430FR2433, MSP430F5132, TIDA-00120, MSP-FET
Tool/software: Code Composer Studio
Hello,
I have built the TIDA-010042 however its not setting the MPP of my solar panel to be 17V, instead it is going down to 13V. The battery voltage is 12.5V and charging slightly.
What could be the cause of this? I uploaded the code on the MSP430F5132 using Spy-Bi wire before putting the chip on the board. The programmer used was MSP-EXP430FR2433.
When I try to upload the code on the board again with the chip on the board I get this error. I connected pins 2 and 3 together on header J3 and pins 1, 2, 3, and 4 on header J4 to 3.3V, SBWTCK, SBWTDIO, and GND respectively on my MSP-EXP430FR2433.
I also need to use the GUI. I have downloaded the TIDA-00120 GUI but needed guidance on how to communicate battery voltage to display on the GUI. Pins 4 and 5 on header J1 are connected where and how?
Thanks,