Tool/software: WEBENCH® Design Tools
Customer reports the following which we have verified;
"Noticed something that looks a little peculiar with a WeBench result. This design was produced by the tool, but the EN pin divider doesn’t seem right. Per the datasheet, the EN pin needs to be greater than at least 1.18V to meet max condition for threshold, yet with an input that could be as low as 5.75 in this instance, the EN pin will only reach a little over 1.12V. Am I reading this correctly?"
Is this something that can be addressed in the tool?
Thanks,
Christian