• TI Thinks Resolved

TIDA-00824: demo

Mastermind 19020 points

Replies: 2

Views: 31

Part Number: TIDA-00824

hi,

I need one TIDA-00824 for demo at customer.

Pls reach me in pvt for the details.

KR

Vincenzo

  • Hi Vincenzo,

    My apologies, but we don't have any demo hardware to share. 

    We recommend customers to use LMT70 or TMP117 on a flex circuit for skin temperature as seen in TIDA-01624. Please have a look at this design.

    thanks,

    ren

  • Vincenzo -

    this reference design is five years old and was not made available as an EVM at that time. Are you expecting to demo the form factor or the performance? 

    there are options if you can just demo the performance

    the design files are online, as you have found and this is made from MSP430G2553, which there is a LaunchPad for and Adafruit makes ADS1115 breakout board, which on their site is out of stock, however they do have stock of the ADS1015 board (12 bit vs 16 bit) 

    MSP430 LaunchPad ==> https://www.ti.com/tool/MSP-EXP430G2ET

    Adafruit ADS1015 board (could pop on ADS1115 or leave it) ==> https://www.adafruit.com/product/1083

    and there is ADS1118 boosterpack which made for K type Thermocouple, but could be hacked to work, too, probably. 

    Furthermore, you could use MSP432P4111 LaunchPad (which has built in 16bit ADC, if that is really needed) and interface to LMT70 or use TMP117 and any MCU. 

    BR-

    Josh