Other Parts Discussed in Thread: EVM430-FR6047, , MSP430FR6047
Hello,
I want to use the EVM430-FR6047 an connect it to the TIDA-Board like discussed in this thread.
Later on i want to measure the flow with two clamp-on transducers on metal-pipes >= DN80. Do you have experiance to connect the transducers with a 50 Ohm Coax cable (RG 58/ 5m or 10m)?
What do I have to do with the resistors in the output-channel (Termination of the transmission line)? Do I have anything else to consider?
I tryed it with a 50 Ohm resistor in the output channel. This is the "best" result I`ve had so far, but unfortunately the result is useless.
Can you imagine the reason for this bad result?
Thanks for your help.
Best regards
Matthias Luzius