Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Is it correct to enter the values of the closed circuit voltage and current parameters of tida-01604 as shown in the picture?
The output of 240V came out in the open loop, but the value of GuiIi is not 1.
Of course, the Open Loop setup is the next guide.
INCR_BUILD is 1: Open Loop and Input VL-L (Vrms) is input as 120.
Looking at the schematic of Tida-01604, Rfltr is 1.4 kOhm and Cfltr is 0.01 uF.
I think you should change the value of "Sensespace's Sense Filter" as follows.
Rfltr: 47 -> 1400
Cfltr: 0.047->0.01
Please check if it is correct. I don't understand, so I don't think sensing works properly when I experiment.
Accurately provide the "workspace parameter" value according to the schematic.