Hello,
I see there are two sets of bleed resistor in the design guide. One on the input side, one on the output side. Why is that? Why can't one set of bleed resistor be sufficient? Why is the input side resistor value so small when C needed to be discharged is lesser on input side?
I have attached an image of the design given in TIDA-00779 too. The question relates to R34, R35, R36, R37, R29, R30, R32, R33.