Texas Instruments (TI) Bluetooth® support forum is an extensive online knowledge base where millions of technical questions and solutions are available 24/7. You can search Bluetooth® IC content or ask technical support questions on everything from BAW resonator technology and Bluetooth® low energy to BLE automotive and wireless connectivity with smartphones & tablets. Find the right solution for your circuit design challenges by using our TI E2E™ support forums that are supported by thousands of contributing TI experts.
Part Number: CC2340R5
Dear users,
IAR Embedded Workbench users are recommend to use IAR 9.40.2 with F3 SDK 7.40.00.64. This information has not been properly reported in the release notes of the SDK.
Using previous IAR versions may lead to issue during…
Part Number: CC2340R5
The purpose of these instructions are to detail how to merge/add multiple BLE profiles into a single project. The following is an example which uses the " data_stream_UART_over_BLE" as the base project and the "basic_ble_profiles…
This guide shows how to use SDK Composer so the size of the SDK downloaded and installed is reduced.
This guide applies to the devices supported by the SimpleLink Low Power F2 SDK (CC13x1, CC13x2, CC13x4, CC26x1, CC26x2 and CC26x4) and SimpleLink Low Power…
Part Number: LP-EM-CC2340R5 Other Parts Discussed in Thread: CC2340R5
The following details how to modify the uart2echo SDK example to enable the event Mask, and event Callback overrun on the LP-EM-CC2340R5.
Summary:
By implementing the following code…
Part Number: CC2642R Other Parts Discussed in Thread: CC2652R , CC2652R7 , SYSCONFIG Hi,
Here are some steps to enable synchronization with a periodic advertising train on CC2642R, CC2652R or CC2652R7.
This guide assumes you are using the simple_central…
Part Number: CC2642R Other Parts Discussed in Thread: CC2652R , CC2652R7 , SYSCONFIG
Hi,
Here are some steps to enable periodic advertising on CC2642R, CC2652R or CC2652R7.
This guide assumes you are using the simple_peripheral example for the device selected…
Part Number: ZIGBEE-POWER-CALC TI is pleased to announce a new TI Arm Clang Compiler Tools release 3.2.0.LTS which includes the following new features.
New features:
Support for ELF Segment "Blocking" (Alignment and Padding)
Support for OpTI…
Part Number: CC2340R5 Other Parts Discussed in Thread: BOOSTXL-AUDIO , SYSCONFIG
Hi,
Here is a step by step guide showing how to use the PWM example to produce a siren-like sound.
The example is based on F3 SDK 7.20.00.29.
A BOOSTXL-AUDIO is used to turn…
Part Number: CC2340R5 Other Parts Discussed in Thread: UNIFLASH ,
Hi,
Here are the steps I recommend to follow to debug the basic_persistent app c (similar steps can be applied for basic_ble_oad_on_chip, basic_ble_oad_off_chip, etc.).
I- Build the image…
Part Number: CC2340R5 Other Parts Discussed in Thread: SYSCONFIG
CC23XX Debug Logging Feature
We have recently released a new debug logging feature on the SimpleLink Low Power F3 SDK for the CC23xx devices . The logging feature allows users to output a debug…