Hy,
in an application I need to record and parse a serial digital signal. My idea is to store the value of a free running counter on every edge of the signal using DMA. When I now parse through the stored values I can retrace the number of Ones and the number of Zeros when I know the ratio of the free running counter and the bit rate of the signal.
- Is it possible to use both edge of a GPIO signal as a DMA trigger?
- Is it possible to do a "8 bit peripheral none increment" to "8 bit memory 1 byte increment ring buffer" DMA transfer?
- Can I poll from software the current target address of DMA to find out if and how many new values have been stored already?
- If yes, is there sample code on how to realize this`?
Best regards
Harald