Hello,
My application is based on project_zero example and has two additional tasks Task_A and Task_B. These tasks should be able to exchange messages and also send/receive messages to/from BLE appTask (not to BLE Stack). I understand that appTask uses ICall interface to exchange messages with BLE Stack.
1. Should Task_A and Task_B use ICall to talk with appTask? If yes, what should be done to enable this iICall for Task_A and Task_B?
2. Which events should be used? Should it be unique event for each one of target task?
3. Is Message Queue should be defined for each one of these tasks or all of them use the same queue?
4. Is there any example of communication and synchronization of application tasks?
Thanks,
Yakov