Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
Hey there,
I am using the CC2640 with simple_central example on a custom board. I would like to change the device name using the -
static const uint8_t attDeviceName[GAP_DEVICE_NAME_LEN] = "PUI Tal O Central ";
GGS_SetParameter(GGS_DEVICE_NAME_ATT, GAP_DEVICE_NAME_LEN, (void *)attDeviceName);
command AFTER the application is up and running after the initial setting in the SimpleBLECentral_init(). Need to get details for name from another processor which is only readable after the system is up and running.
However when I try to write using this function the system gets stuck in the
ti_sysbios_family_arm_m3_Hwi_excHandler__I():
For that matter I get the same response when I try to read this field using -
GGS_GetParameter(GGS_DEVICE_NAME_ATT, (void *)&attDeviceName);
What is the trick to changing the device name at runtime?
Thanks
Fred