Tool/software: Code Composer Studio
Hi,
I am working on modified Project zero version, its working great. We are using open source BLE scanner app to read and write data from our device.
Now I want to try a connection from my mobile to CC2640R2 device without any app. I dont want to read or write data, I just want to make a pairing connection with my mobile just like connecting a Bluetooth headset or some other BLE device pairing with mobile phones.
Is this possible?
I have modified the pairing code in Project zero as below, but that didnt work on pairing with mobile.
The below code is in project_zero.c file under Application folder i project zero example project.
uint32_t passkey = 0; // passkey "000000"
uint8_t pairMode = GAPBOND_PAIRING_MODE_INITIATE;
uint8_t ioCap = GAPBOND_IO_CAP_KEYBOARD_DISPLAY;
Thanks
JanSom