Other Parts Discussed in Thread: CC2650
Hi, i'm gyu yang who using a CC2650 Development Kit with CCSv8.
And i have experienced with advertise Mode because it can find the example code in resource explorer.(with 2 CC2650DK, i set up one is Advertiser(TX), and another is Observer(RX). and succeed to exchange the Advertising Packet in Advertisement mode.)
For using TX/RX advertising Packet, i using these command.
in Tx side
>CMD_RADIO_SETUP executed
> Status: 0x400 DONE_OK
>CMD_FS executed
> Status: 0x400 DONE_OK
>CMD_BLE_ADV_NC executed
> Status: 0x1400 DONE_OK
>CMD_ABORT executed
> Status: 0x1 DONE_OK
in Rx side
>CMD_RADIO_SETUP executed
> Status: 0x400 DONE_OK
>CMD_FS executed
> Status: 0x400 DONE_OK
>CMD_BLE_GENERIC_RX executed
> Status: 0x2 ACTIVE
>CMD_ABORT executed
> Status: 0x1 DONE_OK
__________________________________________________________________________________________________
but, with this mode, the payload data packet(ADV_NONCONN_IND) should be lower than 37 byte. so it's a problem for me.
so i want to change communication type into Connection Mode to increase the payload packet data size. it' means that i want to set up one is Master and another is Slave.
so for doing it, is there example codes concerning about Connection Mode or Materials?
Thanks in advance!