This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 903
Part Number: CC2564C
– The minimum encryption key size used for the LMP_encryption_key_size_req PDU shall be set to at least 7 octets
– All BR/EDR Controllers shall implement the Read Encryption Key Size command (0x1408).
– TI Dual-Mode Bluetooth controllers: CC256x, CC256xB, CC2564C, WL12xx, and WL18xx devices
Note: The current and existing Bluetooth Core Specifications for Low Energy (LE) devices implementing LE Legacy Pairing and LE Secure Connections (LESC) already require a minimum encryption key length of 7 octets and are thus not applicable to Bluetooth Erratum 11838.
Thanks for the info!
-Katie