Other Parts Discussed in Thread: BLE-STACK
Hi,
A customer tried to test "HCI_LE_EnhancedTransmitterTest" over a "ble5stack simple_peripheral -PTM" project. They are using the simplelink_cc2640r2_sdk_2_20_00_49.
The "HCI_LE_EnhancedTransmitterTest" command were sent from BTool(v1.42.10BLE5)
As you see below log, there were no response from the peripheral when the "HCI_LE_EnhancedTransmitterTest" were sent to the peripheral.
please let me know how to clear this issue !
-------------------------------------------------------------------
[3] : <Tx> - 02:05:45.216
-Type : 0x01 (Command)
-OpCode : 0x2034 (HCI_LE_EnhancedTransmitterTest)
-Data Length : 0x04 (4) byte(s)
TxChannel : 0x01 (1)
TestData : 0x0A (10)
DtmPktPattern : 0x00 (0) (Dtm_PRBS9)
TxPhyType : 0x01 (1) (Phy 1 Mbps)
Dump(Tx):
0000:01 34 20 04 01 0A 00 01 .4 .....
--------------------------------------------------------------------
[4] : <Tx> - 02:05:52.269
-Type : 0x01 (Command)
-OpCode : 0x2034 (HCI_LE_EnhancedTransmitterTest)
-Data Length : 0x04 (4) byte(s)
TxChannel : 0x00 (0)
TestData : 0x00 (0)
DtmPktPattern : 0x00 (0) (Dtm_PRBS9)
TxPhyType : 0x01 (1) (Phy 1 Mbps)
Dump(Tx):
0000:01 34 20 04 00 00 00 01 .4 .....
--------------------------------------------------------------------
[5] : <Tx> - 02:06:26.679
-Type : 0x01 (Command)
-OpCode : 0x201E (HCI_LE_TransmitterTest)
-Data Length : 0x03 (3) byte(s)
TX Channel : 0x00 (0)
TestData Length: 0x00 (0)
TestData : 00
Dump(Tx):
0000:01 1E 20 03 00 00 00 .. ....
--------------------------------------------------------------------
[6] : <Rx> - 02:06:26.713
-Type : 0x04 (Event)
-EventCode : 0x000E (HCI_CommandCompleteEvent)
-Data Length : 0x04 (4) bytes(s)
Packets : 0x01 (1)
OpCode : 0x201E (HCI_LE_TransmitterTest)
Status : 0x00 (0) (SUCCESS)
Dump(Rx):
0000:04 0E 04 01 1E 20 00 ..... .
--------------------------------------------------------------------