Other Parts Discussed in Thread: BLE-STACK
Tool/software: Code Composer Studio
Hy,
things have obviously changed since 2.1.0.44423....
Back then, Stack and App have compiled to hex files. I could merge them and, more important, update them separately. Now, with 2.20.00.49 (CC2640R2) it seems, that stack is compiled as library and then linked during build of the application.
Is there a way to change this again? I need to keep devices compatible with some previously defined methods, i.e. a unique revision for the stack and separate OADs for stack and application.
Also, the project files seem different: so far I was used to .ccsproject, .cproject and .project files, now there is xxx.projectspec
Back then I imported the projects as CCS projects, option "Copy projects into workspace" not checked. So physically I was working at the source directory. Now, it seems that projects are always copied into my workspace. When I try to open a project a 2nd time, I get the notice "An eclipse project already exists at location"
What documentation would help me in switching from ble_cc26xx_2_01_00_44423 to simplelink_cc2640r2_sdk_2_20_00_49?
Best regards
Harald