Is there any reference source code available for TRF7970A EVM board ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thank you Ralph for providing the link. I have requested TI to share the files. Hope the request will be approved.
Just to give you little detailed background :-
I am representing a small software service company based in Kolkata, India. I am working for our client with their innovation center at Silicon valley. Our client manufacture proprietary NFC tags (subset of ISO/IEC 14443) using their printed technology. Currently these tags are only working in tag talk first mode and you can only read them (no write). Now they are developing writable tag with proprietary standard.
Earlier we have bought multiple TI TRF7970A EVM boards and developed the client tag reader firmware for our client successfully using DM1. Obviously I have taken help from example base codes from TI document
There were no transmission of read request from TRF7970A as the above tags will spontaneously transmit if they get power from reader.
Now we have new requirement of writable tag. We need to send proprietary read, write, enable, disable etc commands using Modified Miller code at 106 kbps. The printed IC resource is very limited. So we decided to issue very small size commands like 4 bit and 1 bit command / data. Example :-
0 (Sof), 0000 (data), no eof
0 (Sof), 1111 (data), no eof
0 (Sof), 0 (data), no eof
0 (Sof), 1 (data), no eof
I am using SDM mode. But I am unable to eliminate the eof bit (which is always 0) .
So, I am not sure this can be done using SDM (I have already tried few days).
And now thinking to use DM0 for transmitting the very short commands.
BR,
Debojyoti
Images_ModifiedMillerCode_4bit_12Nov2018.zipJust to be more accurate :-
Sof is not start of frame - it is start of communication => Sequence Z
eof is end of communication
Hello Debojyoti,
It should have no issue being approved but the process can be a bit slow. On our teams end the request hasn't made it to us yet, but there is another approval step between your submission and us getting the request. If you still don't have approval by this time tomorrow let me know.
Hello Debojyoti,
I have not and will not review those screenshots, as stated your application is outside of what we will support. We are not going to investigate if SDM can work for your application, but you are free to try using it by following our app note on how to use it for Mifare Classic: http://www.ti.com/lit/pdf/sloa214
The gmail vs company email makes sense, again if you don't get the files within a couple business days then please let me know.
Yes. I have got the code yesterday. Many thanks. Definitely I shall look into it.
However before getting the code I have successfully configured DM0 transmission in slow mode using MOD pin and OOK. I was missing the point that Slave Select to be put low during entire transmission time. Now I have to look into timing as per our client spec.
Many thanks again for helping.
Best Regards,
Debojyoti