This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC-DEBUGGER: CC-Debugger

Part Number: CC-DEBUGGER
Other Parts Discussed in Thread: CC2640, LAUNCHXL-CC2640R2, CC2541

I purchased a CCDebugger along with a stack of other gear to do some development on the CC2640.

It came with a ribbon cable 10 way / 2 row 1.27mm  (The small one not the 2.54mm one) this cable is faulty it has an intermittent short between pins one and 2.

Testing to confirm the short was performed multiple times using various male connectors on each end.

I have explored the TI website but found no information on what to do if I have received faulty goods. Could someone please point me in the right direction to get this sorted out?

I dont know where to buy one of these cables and I have priced up making one myself. as I can only buy this ribbon cable on a 30m reel, it will cost me more than $80 to make an adapter and a couple of weeks to wait for the part.

The worse news is that the short tripped the CC2640R2, this lit back up when I disconnected the ribbon cable and reconnected the USB. I haven't tested to see if the board is damaged yet but I suspect that it might be. And even worse, my custom-made board (the one that I need to develop on) may be damaged which is worth another $500! Hopefully not. But the worst bit for me is that I have dedicated the next month to develop this board. So very much hoping that I can get a replacement connector very quickly.

Thanks