Hi all,
I am trying to use packet sniffer based on the cc2531, using sniffer 2.18.1.
protocol type - generic. we send packets on 2.480 Ghz, baud 250K, 12 bytes data, ID=0, 2 bytes sync, 4 bytes preamble
we do not see anything on screen.
the sniffer recognizes the dongle, but does not open the tabs that enables parameters setup, such as baud rate.
how can I setup the comm parameters, such as baudrate, and others?
maybe another version, older version works?
thanks
Israel