This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CC1352P: minimum voltage of CC1352R

Expert 1040 points

Replies: 2

Views: 42

Part Number: CC1352P

Hi,

1. what is the minimum voltage of CC1352R can transmit/receive RF data and at that  voltage what i/o level?

2. where can i change polling interval in sensor to 5 minutes? There is a minimum(1 second) and maximum(10 seconds) polling interval in sensor. If i change 10 seconds to 5 minutes intervals then my sensor is restarting? what change can be done for this? My application has low power consumption requirement. If i increase polling interval, it will slow sensor receiving message from collector my application is OK with that.

Thanks & Regards

haricharan

  • Hi Haricharan,

    The minimum voltage requirements can be found in the datasheet of the device, the same goes for IO levels.

    As for the sensor questions, it is not very clear what your base point is. I would recommend you create a new thread for this question (as it is two separate questions) where you provide information on what software examples/stacks you are using, SDK versions, and what issue you are seeing. This way, it is easier to get support from the correct subject matter experts.

    Best regards,

    M-W

  • In reply to M-W:

    k thank you for quick response

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.