Other Parts Discussed in Thread: CC1120
Hi,
my customer is asking for a SoC 169MHz band solution.
I don't see it is supported on CC1310 or 1312R1 in datasheet.
do you confirm if it can be extended to there?
BR. Albin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Albin,
There are no plans for CC1310 for 169 MHz.
169 MHz is typically narrowband so recommend the combination MSP430+CC1120 or an offering with BLE support as well: CC2640R2 + CC1120.
What is the requested maximum output power ?
Regards,
Richard