Hi,
I am developing the driver to manipulate the CC1120 chip.
My problem is that I can not get an accurate RSSI value which is provided by the register RSSI1(0x2f71) and RSSI0(0x2f72).
As the datasheet says the resolution of the RSSI is 0.0625dB, but I can not see a one bit change of the RSSI0 register[6:3].
The RSSI_OFFSET is configured around -102dB and CS_THRESHOLD is 0x18, RSSI_VALID_CNT = 2.
How to achieve the designed 0.0625dB resolution?
Thanks
Allen