Tool/software: TI C/C++ Compiler
I'm using a CC1310 with SDK 1.5 and I am tight for RAM space.
My code below required me to change the size of this buffer
//#define BUFF_SIZE 200 //when RCM was added
#define BUFF_SIZE 1050 //fwu
char input[BUFF_SIZE]; //UART buffer
I'd like to be able to change the array size of "input" on the fly, how does TI-RTOS support this?
Also, besides obvious application code practices, are there ways to conserve RAM via the RTOS using switches, or something I am overlooking?
I only have about 2K out of 20K left.
Thanks in advance,