Other Parts Discussed in Thread: TEST2
I have two CC1101's communicating with GFSK at 434 MHz. They are connected to Raspberry Pi's, and use the GitHub SpaceTeddy library.
Since, the CC1101 board and antenna communicates fine at 434 and 315 MHz, does that mean it is likely to work at 345 MHz?
What is required to set 345 MHz ASK?
The goal is to read a 64 bit, manchester encoded signal including start bits, and CRC: