One of my customers is trying to understand the phase noise of the internal synthesizer. We understand that the phase noise profile for a typical fractional-N synthesizer varies from channel to channel.and assume that is also the case for the CC1125 Fractional synthesizer. They have a lot of freedom to choose our one fixed channel anywhere in the 137 to 192 MHz range. For best receiver phase noise, what RF channel and IF should they choose when using the CC1125? Or, can you explain the behavior of the CC1125’s internal dividers so that we can perform our own educated search for the best RF channel and IF? For example, for a given VCO frequency, can you explain how to determine the phase detector comparison frequency? Can it be controlled through some of the For test purposes only, use values from SmartRF Studio registers? The goal is to minimize the total close-in phase noise power within ±60kHz of the L.O.