Hi,
I am programming a device using CC1101.
I am doing the program of the mutual communication between the master and the slave.
Carrier sense was frequently observed on multiple boards on the slave unit side using a CPU debugger.
I tried to stop the career sense function as follows to investigate the problem.
////before////
{CC1100_REG_AGCCTRL1,0x50},
{CC1100_REG_AGCCTRL2,0x03}, // CS thrthold about 61dBm add 2018/03/13
////after////
{CC1100_REG_AGCCTRL1,0x48},
{CC1100_REG_AGCCTRL2,0x00}, // CS cariier sense disabled add 2019/03/14
Then, although it was possible to confirm that the transmission radio wave was output by the spectrum analyzer, Slave Unit could not receive any reply signal from the master unit at all.
Please tell me the register (AGCCTRL1 , AGCCTRL2 and so on) setting to disable only the carrier sense function.
Thanks.