Tool/software: Code Composer Studio
Hi,
I'm using multiple ADC channels. one of them is used by the Sensor controller.
Randomly when using ADC measurement from both sides (MCU and SC, note: HW semaphore is used to determine which is the current controller and work great), I get HW reset.
after investigation of this issue, I'm noticed that the function 'ADCBufCC26X2_swiFxn' in 'ADCBufCC26X2_open' randomly set the 'object->activeSamplebuffer' from normal address to 0XFFFFFFF and then we got assertion.