Tool/software: Code Composer Studio
What I'd like to do, and would love some help with, is:
- Set the sensitivity to a maximum (in order to have the EasyLink RX functions trigger even on noise)
- Why: I wan't to verify that the internal RF circuit of the CC1310 is even running, and that I am able to break somewhere in the EasyLink RX functions.
- Questions: where do I define the sensitivity? Which functions of the EasyLink API would you suggest setting breakpoints inside (I've tried both `rxDoneCallback` and `EasyLink_receiveAsync` already)?
- Verify that my application can receive a packet, and filter based on the IEEE-address (lets talk about this when 1. is fulfilled)
- ... well, if 1. and 2. succeeds, I'm pretty much done . But I'd love to hear if you have any other debugging ideas?
I'm a bit worried that the error may be due to the 24 MHz crystal (don't know why, just a wild idea), so is there a way to verify that the internal RF circuitry is `running`?
Thanks!