• TI Thinks Resolved

CCS/LAUNCHXL-CC1310: Cannot debug Contiki-NG Launchpad solution

Prodigy 110 points

Replies: 16

Views: 207

Part Number: LAUNCHXL-CC1310

Tool/software: Code Composer Studio

I have setup a project in Code Composer following the instructions near the end of the page here .

After building, I can launch a debug session using the .elf file for the cc26x0-web-demo found in examples/platform-specific/cc26x0-cc13x0/cc26x0-web-demo/build/cc26x0-cc13x0/launchpad/cc1310 and it runs to main().

But, if I then continue execution, the debugger no longer seems to be able to break the code and the code is not executing properly as the LED on the Launchpad is not blinking.

Pulling the USB connector out of the Launchpad and then re-plugging, the code seems to run fine (LED is blinking), so this seems to be related to the debugging process.

After stepping through the code, it appears that misoperation begins when the interrupts are re-enabled in this call in soc_rtc_init()

/* Re-enable interrupts */
  if(!interrupts_disabled) {
    ti_lib_int_master_enable();

I do not understand why the code appears to run fine when not trying to debug, but misoperates when debugging.

Any help is appreciated.

  • Hey Simon,

    Please allow me some time to find the expert to assist you with this.

    In the meantime, take a look at the following related post as it may provide some insight: https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz/f/156/t/638371.

    Regards,

    Ammar

    Please click the "This Resolved My Issue" button on this post if it answers your question

  • Hi Simon,

    Could you try the following and see if this helps:

    After starting the debugger session and halting in main(), do a Board Reset by clicking

    • Run -> Reset -> Board Reset (automatic connect/disconnect)

    Then issue a restart

    • Run -> Restart

    You should now be back in main() again. Try to run a as normal.

    Regards,
    Severin Suveren

  • In reply to Severin Suveren:

    No, sorry, that did not help. After completing your steps, I seemed to be stopped at the ResetISR()

    I then hit the Resume button and then all except the Terminate button became greyed out and the board was not executing (no LED blinking.)

  • In reply to Ammar N:

    Based on this advice, I tried taking the "hello_world" ccs example project and then changing the project .out reference to the .elf file generated by my Contiki build. I also removed the hello_world .c files from the project and referenced the contiki_main.c. Then, I prevented the hello_world project from building and just used it to debug. I encounter the same problem as with my original project. Attempting to step past approximately the end of the soc_rtc_init() function (where it renables interrupts) results in ccs not breaking and hitting break shows the PC at location 0x100035fc. Once again, pulling the USB cable out of the launchpad and replugging, the LED starts blinking indicating the Contiki code is running normally. (Re-starting the debug session in ccs and just hitting resume from the start of main does not result in code operation.)

  • In reply to Simon Lightbody:

    Have you tried disabling the Watchdog? The watchdog on CC1310 does not properly pause during debugging, and so I've personally experienced that sometimes I need to completely disable the Watchdog when debugging on CC1310.

    Regards,
    Severin Suveren

  • In reply to Severin Suveren:

    Not sure how the watchdog on/off is controlled on this chip, but it appears that the Contiki code configures the watchdog much later in the initialization than I am having the problem at...

    #if PLATFORM_MAIN_ACCEPTS_ARGS
    main(int argc, char **argv)
    {
      platform_process_args(argc, argv);
    #else
    main(void)
    {
    #endif
      platform_init_stage_one();

      clock_init();
      rtimer_init();
      process_init();
      process_start(&etimer_process, NULL);
      ctimer_init();
      watchdog_init();

    Is there a way I can tell if the watchdog is somehow enabled before (in platform_init_stage_one()?)

  • In reply to Simon Lightbody:

    Watchdog is disabled by commenting out the watchdog_init() line. However, if it crashes before that line executes then it probably isn't the watchdog.

    It is hard to say what the problem is. I just followed the guide again, and was able to debug a CC1310 LaunchPad without any problem. Could you please try to redo the project once more. You could also try out the simplelink platform instead of cc26x0-cc13x0 platform.

    Regards,
    Severin Suveren

  • In reply to Severin Suveren:

    Just looking back through the thread and decided to try this again. The behaviour was a little different than before. When I do Run->Reset->Board Reset(automatic connect/disconnect) and then continue execution, the LED does start blinking on the Launchpad, but if I then Suspend, I end up in the lpm_sleep() function and soon after the resume and suspend icons become greyed out leaving the only option as Terminate.

  • In reply to Simon Lightbody:

    Just did a bit more experimenting and it seems that the Contiki code is still turning on the watchdog despite WATCHDOG_CONF_DISABLE being set to 1 in project-conf.h

    Now the procedure where I download, stop at main(), then Run->Reset->Board reset, then run works and I can suspend and resume code execution ok.

    So, now the only question is why is the extra Run->Reset->Board reset required? I still can't just run from the start of main successfully and cannot debug the startup of the code.

  • In reply to Simon Lightbody:

    WATCHDOG_CONF_DISABLE is only available for the simplelink target. cc26x0-cc13x0 target does not support that configuration flag.

    You describing that doing a board reset and then running seems to indicate that it is properly running now. And, when pausing and being in lpm_sleep() is to be expected as you are pausing execution while the device is in standby. However, this probably causes the watchdog to time out and cause the debug session to crash.

    In order to disable the watchdog with the cc26x0-cc13x0 target, you need to comment out the watchdog_init() function call in main().

    Regards,
    Severin Suveren