• TI Thinks Resolved

CC1310: StandBy Mode or Shutdown Mode

Expert 1335 points

Replies: 53

Views: 375

Part Number: CC1310

I tested the examples to consume as little as possible for my devices. Trying the shutdown mode, it works well and the consumption is really very low. I have a doubt in this feature:

  • I have read that it has the functionality of the reset. Is there a way to avoid resetting it when you wake up?
  • How long should the device wake up from shutdown?

I also tried the example of the standBy and saw that it consumes much less than the shutdown and does not need the reset. How can I send the device to standby by pressing a button and waking it up with the same button? I would like to implement this within the RF_packetRX / TX