Tool/software: Code Composer Studio
Hello,
I want to move to a callback-based SPI transfer. I've been using the blocking mode successfully with my CC1352P1 interfaced with an ENC28j60. I followed the spislave example which uses the callback mode.
A few things I wanted to clarify - will I be able to use the SPI module from different threads/tasks if I use the callback mode?
Another thing - I know the spislave example uses the BOARD_MASTER_READY and BOARD_SLAVE_READY pins to coordinate between the master and slave. I have configured the CC1352P1 as the master and the ENC28J60 as the slave. I cannot program any pins on the slave, so I cannot control the BOARD_SLAVE_READY. I removed all references to the BOARD_MASTER_READY and BOARD_SLAVE_READY and my code disappears when I encounter the spi_transfer code. Either that, or what I'm reading back from registers is not correct. (I was reading back the correct values when in blocking mode) Here's my code :
/* Semaphore to block slave until transfer is complete */ sem_t masterSem; /* * ======== transferCompleteFxn ======== * Callback function for SPI_transfer(). */ void transferCompleteFxn(SPI_Handle handle, SPI_Transaction *transaction) { sem_post(&masterSem); }
My spi_write function :
void spi_write(uint8_t reg, uint8_t data){ //uint16_t controlWord = setBufWriteToAddress(address, data); uint8_t bank_selector = whichBank(reg); if ((bank_selector != 0) && (bank_selector != 1) && (bank_selector != 2) && (bank_selector != 3) && (bank_selector != 4)){ Display_printf(display, 0, 0, "Fatal Error - Wrong Register"); while(1); } selectMemBank(bank_selector); uint8_t address = reg & 0x1f; bool transferOK; masterTxBuffer_eight[0] = 0x2<<5 | (address & 0x1f);//((1<<14) | (address & 0x1F) << 8 ) ; masterTxBuffer_eight[1] = data; memset((void *) masterRxBuffer_eight, 0, SPI_MSG_LENGTH); controlReg.count = SPI_MSG_LENGTH; controlReg.txBuf = (void *) masterTxBuffer_eight; controlReg.rxBuf = (void *) masterRxBuffer_eight; /* Toggle user LED, indicating a SPI transfer is in progress */ GPIO_write(Board_GPIO_LED1, Board_GPIO_LED_ON); /* Bitbanging attempt for Chip Select */ GPIO_write(Board_GPIO_CSN0, 0); /* Perform SPI transfer */ transferOK = SPI_transfer(masterSpi, &controlReg); if (!transferOK){ Display_printf(display, 0, 0, "Unsuccessful SPI transfer\n"); while(1); } else{ /* Wait until transfer has completed */ sem_wait(&masterSem); } /* Bitbanging attempt for Chip Select */ GPIO_write(Board_GPIO_CSN0, 1); GPIO_write(Board_GPIO_LED1, Board_GPIO_LED_OFF); sleep(0.5); }
How I opened the SPI module :
/* Open SPI as master (default) */ SPI_Params_init(&spiParams); spiParams.dataSize = 8; spiParams.frameFormat = SPI_POL0_PHA0; spiParams.bitRate = 8000000; spiParams.transferCallbackFxn = transferCompleteFxn; spiParams.transferMode = SPI_MODE_CALLBACK; masterSpi = SPI_open(Board_SPI_MASTER, &spiParams); if (masterSpi == NULL) { Display_printf(display, 0, 0, "Error initializing master SPI\n"); while (1); } else { Display_printf(display, 0, 0, "Master SPI initialized\n"); }
Please let me know what could be going wrong.
Warm regards,
Samyukta