Other Parts Discussed in Thread: CC1312R, MSP430FR2355,
Tool/software: TI C/C++ Compiler
Am just starting out with this part and CCS. The example compiles and loads OK. But I can not connect to any uart. Windows 10 Device Manger shows:
Questions:
1) Which port is used to "talk" to the launchpad system that can configure, load and debug the C1312R ? When I try to connect to COM3 with TeraTerm, it says it can't connect.
2) Please explain what the use of these two ports are and how they are used.
3) In the code uartecho.c, there is a line of code:
uart = UART_open(CONFIG_UART_0, &uartParams);
Where does the constant CONFIG_UART_0 come from? I've looked at all the various .h files (quite the rabbit hole there....) and can't find it.
TIA