This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 14
Views: 2313
Hello,
I am running the "Getting Started with WLAN Station" program but I cannot get any console output. I have a console running for ALL the possible ports, MSP Application UART1, MSPDebug Interface and Communications Port, at 9600, 8, 1 but I do not get any console output.
Any help would be greatly appreciated.
Kas
Hi Kas,
You should connect to the MSP Application UART1 port with terminal settings described in this page.
Did you load the project located in <cc3100 SDK installation locaion>\cc3100-sdk\platform\msp430f5529lp\example_project_ccs\getting_started_with_wlan_station ?
Thanks for posting on TI E2E forum. We appreciate your feedback!Victor Lin
----------------------------------------------------------------------------------------------------- ** Please click the Verify Answer button on this post if it answers your question. **Don't forget to check out our wiki page for lots of useful info: Wireless Connectivity Platforms-----------------------------------------------------------------------------------------------------
In reply to Victor_Lin:
Hello Victor,
I have set the terminal up as explained on that page and I have loaded the project from the suggested location. I have followed the instructions as laid out in CC3100 SimpleLink Wi-Fi and IoT Solution Getting started guide - Users Guide (Doc Ref# SWRU375) but I still do not see anything on any of the possible com ports.
Any further suggestions would be welcomed.
Thanks
I must have been looking at some other code because at closer inspection there is no output in this code. The notes says there is and by all accounts there should be but I can not see anything in main(). So I will put it down to me looking for something which is just not there.
In reply to Kas Lewis:
For Getting Started with Wlan example uart prints are enabled on SDK 0.5.2.
If you are using SDK 0.5.2 you should be able to see the prints.
Regards,
Ankur
----------------------------------------------------------------------------------------------------------Please click the Verify Answer button on this post if it answers your question.----------------------------------------------------------------------------------------------------------
In reply to Ankur Baranwal:
Thank you Ankur,
I will look again as to why it does not appear to be in my code, I will try find a version number somewhere, if you could possibly point me to a location to find this info it would be great.
PS found it in a readme file in ../cc3100-sdk
================================================================================
CC3100 SDK v0.5.2 release================================================================================
Hello Ankur,
I was able to get an output but it stops half way:
Getting started with station application - Version 1.0.0******************************************************************************* Device is configured in default state Device started as STATION
After that there is nothing more. I have started debugging the code but I can't see any the obvious at this point why the CC3100 should not be connecting to the AP.
I think I may have been experiencing a similar issue, I wasn't able to get any output in Tera Term eventhough the COM port settings were correct.
Have you tried connecting with your terminal program after hitting the "debug" button in CCS (but before hitting resume button)? I was able to get the serial output working by doing this.
Cheers,
-Edgar
In reply to Edgar Wong Baxter Jr.:
Hello Edger,
I will give that a try, thank you. A side question, did you have any issues with the other sample projects such as code limit reached with "get_time" or any other issues.
I haven't had any thus far, but lemme try them all tonight and I'll let you know if I come across anything.
That would be great, thank you. I tried Getting time on my home PC with few issues but at work I get a code limit reached error, so I was just wondering.
Thanks so much for the help.