This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200/CC3220: Energia Questions Please read

Mastermind 26340 points

Replies: 1

Views: 6880

Part Number: CC3200, CC3220

The SimpleLink WiFi API that is used for general development is very different from the Energia WiFi API. The programming interface to the CC32XX hardware is very different as well. There are many capabilities that are present using the SimpleLink WiFi SDK that are not available with the Energia environment.

For Energia programming questions, the main energia forum is here: http://forum.43oh.com/forum/125-energia-tivaccc3xxx/

Otherwise, questions about technical details of the CC32XX/CC31XX devices can be asked here.

  ***  Please click the Verify Answer button on a post if it answers your question.   ***
                                                                                                                                         

1 Reply

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.