Other Parts Discussed in Thread: CC31XXEMUBOOST, UNIFLASH
Hi
This is my first post so please bear with me.
I have a design that uses a CC3100R11MRGC connected to a STM32F407 microcontroller via the HOST_SPI bus.
Our implementation is based on the TI BoosterPack™ plug-in module for the hardware around the CC3100 (CC3100 and SPI Flash...).
Our application uses the CC3100 as an Access Point and the only setting we allow is the channel select for a few of the channels, all other Wi-Fi settings are fixed.
We are busy with FCC certification and have been asked to provide the ability to control certain functions of the radio for the testing process.
What is the easiest way to achieve this?
Can I do this without having to develop code for the STM32F407 microcontroller?
Any help greatly appreciated.
Cheers
BJ