This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC3XXXRADIOTEST: Missing .sli for CC3120/ CC3220R

Part Number: CC3XXXRADIOTEST
Other Parts Discussed in Thread: CC3120, CC3220S, CC3220R

Tool/software: TI-RTOS

Hello

After installing ,   radio tool of CC3120_CC3220_RadioTool_1.0.2

I found CC3220S_device_radiotool.sli and CC3120_CC3220_RadioTool_1.0.2, but could not find .sli for 3120 (Booster pack) nor 3220R EVM.

Can you please advise what files to be flashed for 3120 / 3220R to use Radio tool?

Regards,

A.Fujinaka

  • Hi Akihiko Fujinaka,

    The CC3120 doesn't needs anything on the flash other than the latest SP. The PC applications is directly connected to the network processor through SPI (or UART) and send the NWP commands directly.

    The CC3220R will use the same image (.sli) as CC3220S.

    Br,
    Kobi