Hello everyone, I'm thinking of shifting from my cc3200 to cc3220s launchpad but I'm a bit confused evaluating
cc3220s and cc3200sf when it comes to understand how many flash resides on each one.
The problem is that both of ti pages provide the link to the very same hardware overview and schematic:
CC3220 SimpleLink™ Wi-Fi® LaunchPad™ Development Kit Hardware User's Guide (Rev. B)
CC3220 SimpleLink™ Wi-Fi® and Internet of Things Hardware Design Files (Rev. A)
where we can contemplate 4MB flash on board. Long story, but I have the following questions so far.
Does the 3220s lp have 4MB flash ?
If yes, will I be able to store there my specific file and persist my own data as I did in case of 3200 ?
Will I be able to migrate smoothly my 3200 code to 3220s ?