Other Parts Discussed in Thread: WL1837
Hi,
In my project I have to select the channel, wireless standards(a, b, g, n), data rate of the WL1837 wifi device. The wifi is up and running and I am able to scan and connect with wireless AP. Also the iw tools shows that automatically some channel, data rate are selected. I would like to know if I can select the standard(a, b, g, n), channel and the data rate of the device and if so, how can do it?
In between, the "iw reg get" command is giving the below output and I am not able to set any other region.
global
country 00: DFS-UNSET
(2402 - 2472 @ 40), (6, 20), (N/A)
(2457 - 2482 @ 20), (6, 20), (N/A), AUTO-BW, PASSIVE-SCAN
(2474 - 2494 @ 20), (6, 20), (N/A), NO-OFDM, PASSIVE-SCAN
(5170 - 5250 @ 80), (6, 20), (N/A), AUTO-BW, PASSIVE-SCAN
(5250 - 5330 @ 80), (6, 20), (0 ms), DFS, AUTO-BW, PASSIVE-SCAN
(5490 - 5730 @ 160), (6, 20), (0 ms), DFS, PASSIVE-SCAN
(5735 - 5835 @ 80), (6, 20), (N/A), PASSIVE-SCAN
(57240 - 63720 @ 2160), (N/A, 0), (N/A)
Regards,
Pratheesh