Other Parts Discussed in Thread: UNIFLASH, , CC31XXEMUBOOST,
Hi,
I am testing the radio tool for CC3120. I have a setup with CC31xxEMUBOOST and custom board with CC3120R. I can connect to CC3120R with UniFlash tool and program CC3120, but I am having problem to connect CC3120 with Radio tool (v1.0.3.11). I do have RTS and CTS connected to CC3120. the service pack I used in the Wifi image is sp_3.10.0.5_2.0.0.0_2.2.0.6.
My question here is, does this combination works? I see some TI docs mentioned that the correct service pack need to be programmed to use for Radio tool. can someone confirm if the service pack I am using is correct?
another question is, should I just program CC3120 with service pack only?
Thanks,
Jeff