• Resolved

CC3235MODSF: Transmitting at 2.4 GHz and 5 GHz at the same time

Prodigy 120 points

Replies: 1

Views: 46

Part Number: CC3235MODSF

Hi Team,

My customer wants to know if the CC3235MODSF can transmit at 2.4 GHz and 5 GHz at the same time. 

I am assuming it cannot because it is only a single radio, but we wanted to know if this could be dynamically switched at run time.

For example, send a 2.4GHz packet then switch (on the fly) to 5GHz and send a 5GHz packet. In that case, how long does it take to switch from 2.4GHz to 5GHz mode, and vice-versa?

Is it possible to run at 2.4 GHz and 5GHz "at the same time?"

Thanks,

Zack

  • Zack,

    Using both 2.4 GHz and 5 GHz simultaneously is not supported. With 5 GHz enabled, you are able to connect to either 2.4 or a 5 GHz network, but you stick with whatever frequency the SSID you connect to is using.

    Best Regards,

    Vince