Hi TI team,
This is Manjunath, Hardware engineer from Crevavi Technologies pvt ltd, Mysore
We have got a new requirement which is WiFi-Based indoor asset tracking for medical equipment in the hospital,
As I gone through the TI.com website I found CC3120MOD module suits,
Below are our target requirements:
- The tags should be very very small
- Need battery life of 5 years (the battery can be recharged onboard using something – we need to discuss)
- Should withstand chemical cleaning (bleach etc)
- Should be low cost.
- These tags will directly work with the Wifi routers in the Customer locations (hospitals)
- The tags will be used on IT (Laptop, desktops etc) and non IT medical devices (such as IV pumps)
Here the main concern is the battery life, Need a small battery with long life.
So here We need to consider the power saving modes in the Wifi module carefully and we should come out with the what is the battery spec and its life time with respect to the broadcast/advertising interval.
Current frequency of data transmission to be considered is 5min.
Please help us calculating the battery spec.
Thanks
Manjunath
Hardware Engineer
Crevavi Technologies pvt ltd, Mysore