Hi,
I have a problem with WiFi provisioning when I connect mobile phone under Android One to my device which is in Access Point mode. Internet explorer answers: there is no answer from the server.
At the same time, I can connect to this device from the other phones which is not under Android One.
I can see this problem only when I use Android One.
The device on the base of SoC CC3220MODASF12MONR.
Android One version 9 (latest release 1.180904.001).
I use SP sp_3.13.0.3_2.0.0.0_2.2.0.6.bin. Also tried sp_3.12.0.1_2.0.0.0_2.2.0.6.bin and nothing changed.
Can you provide me any ideas how to fix the problem?
Thank you in advance!
Andrey Tikhonov