Hi,
I'm currently using auto+fast connect on our product which works fine in 99% of cases as our products are stationary.
However when a device is configured initially close to an access point, and then moved to the limit of this same access point's range, the device will still connect to it as long as it is detected (even when a much better AP is available)
Is there a recommended strategy to handle this?
If there is not, I'm thinking of periodically doing a scan and doing a manual connection to the best AP. The easiest would be to delete/reset the fast connect stored profile (as the auto profile does just that), is there a way to do this? (Even in a hackish way by deleting the fast connect file?)
Thanks,
Cédric