Tool/software: TI C/C++ Compiler
Dear Community,
I using CC3220s
I have to use low power Wi-Fi.
The cc3220s is known to use LSI mode.
when connected to my Wi-Fi Ap, It was reduced to about 120 uA using the source below.
====================================================================================================================
PmPolicyParams.MaxSleepTimeMs = 1000;
sl_WlanPolicySet(SL_WLAN_POLICY_PM, SL_WLAN_LONG_SLEEP_INTERVAL_POLICY, (uint8_t *)&PmPolicyParams, sizeof(PmPolicyParams));
====================================================================================================================
However, when aws mqtt is connected, using the above source increases to about 16mA.
How to reduce the current to about 120uA when connecting aws mqtt?
thanks.