This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CC2530: ztool

Intellectual 790 points

Replies: 1

Views: 159

Part Number: CC2530

hello, I use ztool for connecting coordinator and router, but there is a problem, in https://sunmaysky.blogspot.com/2017/02/use-ztool-z-stack-30-znp-to-set-up.html 

<TX>03:20:13.59 COM3 UTIL_GET_DEVICE_INFO (0x2700)

<RX>03:20:18.76 COM3 UTIL_GET_DEVICE_INFO_RESPONSE (0x6700)
    Status: SUCCESS (0x0)
    IEEEAddr: 0x00124B00094B7997
    ShortAddress: 0xFFFE
    DeviceType: COORDINATOR, ROUTER, END_DEVICE (0x7)
    DeviceState: DEV_HOLD (0x0)
    NumAssocDevices: 0x00
    AssocDevicesList

and don't get ZDO_END_DEVICE_ANNCE_IND at the end.

where is the problem???

so thanks.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.