Other Parts Discussed in Thread: Z-STACK
We have three CC2530 ZigBee devices in three different locations. Two of them are using ZNP as their firmware. One of the devices is configured as a coordinator, and the other one is an end device. In this scenario, everything works fine and two devices exchange data properly.
However, we have another ZigBee end device which is attached to door with an unknown firmware. The connection between this device and the coordinator has been established without no problem, but the coordinator can not receive any data from the device which is attached to the door. We already checked the packets which are sent from the door device by making use of "Packet Sniffer". The log file of this program has been attached for more information.
The question is, why doesn't the coordinator receive any data?
Sincerely, AmiraPrisha.