This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538: Coordinator start a new PANID network after set ZDSECMGR_TC_DEVICE_MAX=150 in Z-Stack 3.0.1

Part Number: CC2538
Other Parts Discussed in Thread: Z-STACK

Hi All,

I'm using CC2538 as the Coordinator to setup a big network. I set the ZDSECMGR_TC_DEVICE_MAX to 150 on CC2538 in Z-Stack 3.0.1.

NV_RESTORE is enabled in my project.

When I power up the CC2538, it will create a new PANID network first time.

When I power cycle the device, it will create another new PANID network. 

I'm confused why it create a new network PANID.

Thanks.