Tool/software: Linux
in Contiki3.0 I want build rpl-border-router in cc2530dk (path: Contiki3_0Test/release-3-0/examples/ipv6/rpl-border-router)
and I use the command to build => make TARGET=cc2530dk border-router.hex
and I can't build success.
If i have any wrong ? Why can't I build it success
error log :
../../../core/net/ipv6/uip-ds6-route.c:322: syntax error: token -> 'const' ; column 7
../../../core/net/ipv6/uip-ds6-route.c:323: error 20: Undefined identifier 'nexthop_lladdr'
../../../core/net/ipv6/uip-ds6-route.c:380: error 20: Undefined identifier 'nexthop_lladdr'
../../../core/net/ipv6/uip-ds6-route.c:380: warning 127: non-pointer type cast to generic pointer
from type 'int fixed'
to type 'struct __00010006 generic* fixed'
../../../core/net/ipv6/uip-ds6-route.c:389: error 20: Undefined identifier 'nexthop_lladdr'
../../../core/net/ipv6/uip-ds6-route.c:389: warning 127: non-pointer type cast to generic pointer
from type 'int fixed'
to type 'struct __00010006 generic* fixed'
make: *** [obj_cc2530dk/uip-ds6-route.rel] Error 1